Standard Gas Cylinder records store details about a gas cylinder of known components that is used to calibrate a device.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
The following table provides an alphabetical list and description of the fields that exist for the Standard Gas Cylinder family. The information in the table reflects the baseline state and behavior of these fields.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Actual Sample Volume | Numeric | The volume of the sample in the cylinder. | You can enter a value manually. |
Cylinder Connection Number | Character | A number that represents the cylinder connection specification as per standards. | This field appears as a list that is populated by the MI_GAS _CYLINDER_CONNECTION_NUMBER System Code Table. |
Cylinder Description | Character | A description of the cylinder. | You can enter a description of the cylinder. |
Cylinder Identification Number | Character | The ID of the cylinder. |
You can enter a value manually. This field is required. |
Cylinder Manufacturer | Character | The manufacturer of the cylinder. | You can enter a value manually. |
Cylinder Owner | Character | The person who is responsible for the cylinder. | You can enter a value manually. |
Cylinder Size | Character | The size specifications of the cylinder. | This field contains a list of specifications from which you can select the appropriate size. This field appears as a list that is populated by the MI_GAS_CYLINDER_SIZE System Code Table. |
Cylinder Type | Character | The type of the cylinder. | This field appears as a list that is populated by the MI_GAS_CYLINDER_TYPE System Code Table.This field contains a list of types from which you can select the appropriate Calibration type. |
Expiration Date | Date | The date on which the cylinder can no longer be used. | You must select a date using the calendar. |
In Service Date | Date | The date on which the cylinder became available for use. | You must select a date using the calendar. |
Laboratory Number | Character | The number assigned to the cylinder for testing in a laboratory. | You can enter a value manually. |
Min Cylinder Pressure | Character | The minimum acceptable pressure that must be maintained in the cylinder. | You can enter a value manually. |
Copyright © 2018 General Electric Company. All rights reserved.