Standard Gas Component records store details about a gas component that is part of a standard gas cylinder.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
This topic provides an alphabetical list and description of the fields that exist for the Standard Gas Component family. The information in the table reflects the baseline state and behavior of these fields.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Analytical Result | Numeric | The concentration of the component as found by third party verification. |
This value must fall within the tolerance that you have specified for the value in the Requested field. For example, consider the following values:
Then, the value in the Analytical Result must fall between 59 ppm and 61 ppm. Otherwise, an error message appears. |
Balance | Boolean | Indicates whether the component is the balance component. | You can select only one component as balance among all the components in the cylinder. |
Component | Character | The name of the component. | This field appears as a list that is populated by the MI_CHEMICAL_COMPONENTS System Code Table. The component that you select must be unique among the ones linked to the same Standard Gas Cylinder. |
Cylinder ID | Character | The ID of the Standard Gas Cylinder record that is linked to this Standard Gas Component record. | This field is disabled and populated. |
Requested | Character | The concentration of the component that has been requested. | You can enter a value manually. |
Tolerance | Numeric | The percentage of variation from the specified value of the composition of the component. | You can enter a value manually. |
Units | Character | The units of measure for the composition of the component. |
Select from the list of values that have been specified in the system code table. |
Copyright © 2018 General Electric Company. All rights reserved.