The following baseline record states are configured for the Calibration family:
In Progress: Indicates that the Calibration is in progress or yet to be sent for approval. You can modify a Calibration only if it is in the In Progress state. After you have entered all the required information in the Calibration, you can send it for approval by changing the state to Pending Approval.
Pending Approval: Indicates that the Calibration has been sent for approval. If you are a member of the MI Calibration Administrator Security Group, you can approve or reject the Calibration. If you approve the Calibration, the state of the Calibration changes to Approved. If you reject the Calibration, the state of the Calibration changes to In Progress.
Approved: Indicates that the Calibration has been approved. After the state of a Calibration is set to Approved:
The associated Calibration Task is cycled. That is, the Last Date field is set to the date on which the state of the Calibration is set to Approved. The Next Date field is set to the date on which the Calibration must be performed again (in case of a recurring task).
The Calibration is closed.
You cannot delete the Calibration.
Illustration of the Calibration State Configuration
By default, the following baseline State Configuration exists for the Calibration family: