Unit Strategy Records

The following table provides an alphabetical list and description of the fields that exist in the Unit Strategy family. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Description Text A description of the Unit Strategy. The Text Editor window appears, on which you can enter your description.
Risk Analysis Type List A value that indicates whether the strategy results (shown in the graphs) are based on an ASO Analysis or not.

The field will contain one of the following values:

  • Simulation: The strategy results are based on an ASO Analysis.

  • Qualitative: The strategy results are not based on an ASO Analysis.

Note the following about the Risk Analysis Type field:

  • If the Unit Strategy has never been used to create an ASO Analysis, the value will be set to Qualitative, and the field will be disabled. The value will be changed automatically to Simulation if you create an ASO Analysis from the Unit Strategy.

  • If the Unit Strategy was used to create an ASO Analysis, the value will be set to Simulation, and the field will be enabled. If needed, you can change the value to Qualitative to update the strategy results so that they are no longer based on the ASO Analysis. If you change the value to Qualitative, the ASO Analysis will not be deleted or unlinked from the Unit Strategy.

Unit ID

Character The ID of the Unit Strategy. Does not have to be unique. This field is required.

Copyright © 2018 General Electric Company. All rights reserved.