The following table provides an alphabetical list and description of the fields that exist in the Asset Strategy family. The information in the table reflects the baseline state and behavior of these fields.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Description | Text | A description of the strategy. | The Text Editor window appears, on which you can enter a description. |
Plan Length | Numeric | The number of years for which you want to calculate costs. | This value will be used to determine the number of datapoints (bars) on the Cost Projection graph. |
Risk Analysis Type | List | A value that indicates whether the strategy results (shown in the graphs) are based on an ASO Analysis or not. |
The field will contain one of the following values:
Note the following about the Risk Analysis Type field:
|
Strategy ID |
Character | The ID of the strategy. | Does not have to be unique. |
Strategy Notes | Text | Any additional information you want to provide about the strategy. | The Text Editor window appears, on which you can enter any notes. |
Strategy Re-Evaluation Date | Date/Time | The date on which you want to reevaluate the strategy. | Cannot be before the Activated By date. |
Copyright © 2018 General Electric Company. All rights reserved.