The following table provides an alphabetical list and description of the fields that exist in the Action family. The information in the table reflects the baseline state and behavior of these fields.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Action Basis | Text | The basis for the action being created. | This is not a required field. |
Action ID |
Character | The ID of the action. | Populated automatically from the name of the associated strategy when the action is created. |
Action Type | List | The type of action you are creating. | Use the drop-down list to select the type of action. |
Condition Monitoring Type | List | The type of condition monitoring for the action. | This field becomes active after the associated strategy is moved to an Active state. |
Cost | Numeric | Cost to execute the action in US dollars. | Every time the action is performed, this amount is factored into the Annual Cost and Cost Projection graphs. |
Cost Basis | Text | Description to justify cost of performing action. | Enter basis for the cost of carrying out the action each time. |
Description | Text | A description for the action. | This is not a required field. |
Existing Plan | Boolean | Is this action part of an existing plan? | Select the check box if the action is part of an existing plan. |
Interval | Numeric | The number of the interval unit corresponding to how often the action should be performed. | This value corresponds with Interval Units to give the complete frequency with which the action should be performed. |
Interval Units | List | The unit of the interval corresponding to how often the action should be performed. |
This value corresponds with Interval to give the complete frequency with which the action should be performed. |
Mandatory | Boolean | The action is required. | This check box is filled if the action is a required action. |
Name | Text | A name for the action. |
This is a required field. |
Nonrecurring | Boolean | Should the action be on a recurring basis or only once. | Select the check box if you only want the action performed once instead of on a recurring basis. |
Performance Interval | Numeric | Reference value for the interval of the performance of the action. | The values in the Performance Interval field is not used in any calculations in ASM. You can use them as reference values, but no logic is executed based on the values. All calculations that require an interval are based on the values in the Interval field and the Interval Units field. |
Performance Interval Units | List | Reference value for the interval units of the performance of the action. | The values in the Performance Interval Units field is not used in any calculations in ASM. You can use them as reference values, but no logic is executed based on the values. All calculations that require an interval are based on the values in the Interval field and the Interval Units field. |
Recommended Resource | Text/List | A custom entry for a resource to execute action. | Use the drop-down list and enter text into the add caption box that corresponds to the custom resource. |
Shutdown Required | Boolean | Is shutdown required after performing the action? | Select the check box to flag for an equipment shutdown after the action is applied. |
Target Completion Date | Date/Time | Target date for the action to be executed. | Use the date/time selectors to select the date and time by which the action must be executed. |
Copyright © 2018 General Electric Company. All rights reserved.