About Risks and Actions

A risk identifies a way that a location or a piece of equipment can fail, as well as the consequence of the failure. This consequence is presented as a risk rank value, which is determined from the values that you select in the Risk Assessment interface that appears when you create a risk. After you have created an Asset Strategy record, you can begin adding risks to the asset strategy.

The values that you specify in a risk are stored in a Risk record. Throughout this documentation, unless it is necessary to refer to the record itself, we use the term risk.

An action identifies the physical ways in which you maintain a piece of equipment or location. For example, an action might indicate that you want to perform a visual inspection of a piece of equipment. After you have created an Asset Strategy record, you can begin adding actions to the asset strategy.

The values you specify in an action are stored in an Action record. Throughout this documentation, however, unless it is necessary to refer to the record itself, we use the term action.

Switch the Positions of the Risks and Actions Columns

In the Risks and Actions workspace, you can switch the position of the risks and actions columns by selecting .

Whichever column appears in the left side of the workspace, Risks or Actions, is in the primary position and is selectable. This means that, for example, if the Risks column is on the left and you select a particular risk, all the actions that mitigate that risk appear in the Mitigating Actions column on the right. Similarly, if the Actions column is on the left and you select a particular action, all the risks that are mitigated by that action appear in the Mitigated Risks column on the right.

Expand Risks and Actions Cards

The cards in the Risks and Actions workspace can be expanded to display more details by selecting , and then collapsed by selecting .

When you expand an Action card, the following information is displayed:

When you expand a Mitigating Action card, the following information is displayed:

When you expand a Risk card, the following information is displayed:

When you expand a Mitigated Risk card, the following information is displayed:

Sort Risks and Actions

Risks and actions can be sorted to display the items that you are most interested in viewing from a large list by selecting .

In the Sort List By box, you have the following options:

As you make selections in the Sort List By box, the grid sorts accordingly.

View Changes to a Modified Strategy

You can view a summary of the changes made to a modified strategy by selecting XX Action Changes at the upper-right area of the strategy record. When you select it, the Changed Actions window appears, listing the actions and fields that have changed on the left and the read-only Basis For Revision/Rework on the right. If a strategy is in a Pending Review state, the Basis For Revision will appear. If a strategy is in a Modified state, having gone through a rework, the Basis For Rework will appear. Only actions that have changed appear in the list of fields; not risks.

Modifying Risks, Actions, and Assessments

When an action or a risk appears in the right column of the grid in the Risks and Actions workspace, the status displayed is the status of the Risk Assessment. The following table lists examples of operations and their resulting statuses.

Operation Resulting Status in the Right Pane
Modify a risk or action directly without affecting the assessment. No status icon will be displayed.
Modify the assessment without modifying the risk or action. Status icon will be .
Link an existing action or risk. Status icon will be .
Link a new action or risk. Status icon will be .
Unlink an existing assessment. Status icon will be .
Unlink a new assessment. Risk or action card will no longer be displayed.
Delete an existing risk that has mitigating action(s). Status icon will be .

Copyright © 2018 General Electric Company. All rights reserved.