Health Indicator Mapping Records

This topic provides an alphabetical list and description of the fields that exist for the Health Indicator Mapping family, whose records are used to determine how values will be mapped from health indicator source records to the Health Indicator records that they are used to create. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.

Field

Data Type

Description

Behavior and Usage

Asset to Source Relationship Family ID

Character

The relationship family used to link the Equipment record to the health indicator source record.

The list in this field contains all Relationship families delivered in the baseline database.

This field is required.

Description

Character

The purpose of the Health Indicator Mapping record.

This value is not used when mapping data from health indicator source records to Health Indicator records.

Family ID

Character

The family caption of the health indicator source family.

The list in this field contains all families that are successors to the Health Indicator family through the Health Indicator Has Source relationship.

List of Values Field

Character

The field in the health indicator source family that specifies the values that are valid to be entered into reading source records.

For example, Measurement Location records (health indicator source records) can accept either numeric or character values. If they are configured to accept character values, the Allowable Values field in the Measurement Location record stores values that are valid to be entered in the Reading records (reading source records) to which it is linked.

The list in this field contains fields that are stored in health indicator source records.

Mapping Type

Character

The type of data that will be evaluated in the health indicator source record to determine the status of the Health Indicator record.

The list in this field contains the values Character and Numeric.

Reading Date Field

Character

The field in the reading source family that contains the date associated with a reading.

The list in this field contains fields that are stored in reading source records.

Reading Family ID

Character

The reading source family that contains the value that the GE Digital APM rule logic will use to determine the status of the Health Indicator record.

The list in this field contains all families that are successors to the health indicator source family through any relationship.

Reading UOM Field

Character

The unit of measure that is associated with the reading source record.

The list in this field contains fields that are stored in reading source records.

Reading Value Field

Character

The field in the reading source family that contains the reading value that the GE Digital APM rule logic will use to determine the status of the Health Indicator record.

The list in this field contains fields that are stored in reading source records.

Source Name Field

Character

The field in the health indicator source family whose value will be mapped to the Name field in the Health Indicator record that is created.

The list in this field contains fields that are stored in health indicator source records.

Target Field

Character

This field is not currently used.

N/A

Type Field Character The field in the health indicator source family that indicates the type of reading that is associated with a health indicator source record.

When a new entity or relationship record is added to the database, the Asset Health Indicator service compares the contents of the specified Type Field to the value in the Type Value field. If the values match, a Health Indicator record is created automatically using this Health Indicator Mapping record.

If the Type Field and Type Value fields are not specified, a Health Indicator record will be created for each Health Indicator Mapping record that is configured for the health indicator source family.

Type Value Character The value that the specified Type Field must contain in order for this Health Indicator Mapping record to be used. See Type Field.

Copyright © 2018 General Electric Company. All rights reserved.