MI MOC Exception records store information about Exceptions that you created. The MI MOC Exception family is also used in the MOC module to store information about the Exceptions that are associated with a Change Project. This topic provides an alphabetical list and description of the fields that exist for the MI MOC Exception family and appear on the MI MOC Exception datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive, and contains only those fields that are used in the Application Settings for Management of Change.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Description | Character | The description of the Exception. | You can enter a value manually. |
Exception ID | Character | The identification of the Exception. |
This field is required. You must enter a unique value in this field. On the datasheet, this field is labeled as Exception. |
Exception Type | Character | The type of Exception. | You can enter a value manually. |
Is Admin Setting | Boolean | Indicates whether the Exception represents a record created in the Application Setting. |
This field does not appear on the datasheet. The value in this field is True for an Exception that you created in the Application Settings for Management of Change. The value in this field is False for an Exception that is created automatically based on your response to a Checklist Question in a Change Project. |
Copyright © 2018 General Electric Company. All rights reserved.