MI MOC Checklist Question records store information about the Questions that you created for a Checklist. The MI MOC Checklist Question family is also used in the MOC module to store information about the Checklist Questions that are associated with a Checklist of a Change Project. This topic provides an alphabetical list and description of the fields that exist for the MI MOC Checklist Questionfamily and appear on the MI MOC Checklist Question datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive, and contains only those fields that are used in the Application Settings for Management of Change.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Checklist Question ID | Character | The identification for the checklist question. |
This field is required. You must enter a unique value in this field. On the datasheet, this field is labeled as Question. |
Description | Character | A description for the question. |
You can enter a value manually. |
Is Admin Setting | Boolean | Indicates whether the Question represents a record created in the Application Setting. |
This field does not appear on the datasheet. The value in this field is True for a Question that you created in the Application Settings for MOC. The value in this field is False for a Question that is automatically created by GE Digital APM as a copy of a Question that you created. |
Question Text | Character | The text for the Question. |
This field is required. You can enter a value manually. |
Copyright © 2018 General Electric Company. All rights reserved.