MI MOC Checklist Question records store information about the Checklist Questions that are associated with a Checklist of a Change Project. When you add a Checklist to a Change Project, MI MOC Checklist Question records are created automatically by copying the Checklist Question records that you created in the Application Settings for MOC. This topic provides an alphabetical list and description of the fields that exist for the MI MOC Checklist Question family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Checklist Question ID | Character | The identification for the Checklist Question. |
This field is automatically populated with a unique value. |
Description | Character | The text of the Checklist Question. |
This field is populated with the value in the Description field of the MI MOC Checklist Question record whose copy is being created. |
Is Admin Setting | Boolean | Indicates whether the Checklist Question represents a record created in the Application Setting. |
This field does not appear on the datasheet. This field is True if you created the record using the Application Settings for MOC. This field is False if GE Digital APM automatically created the record as a copy of the Checklist Question that you created. |
Question Text | Character | The text for the Checklist Question. |
This field is populated with the value in the Question Text field of the MI MOC Checklist Question record whose copy is being created. |
Copyright © 2018 General Electric Company. All rights reserved.