MI MOC Checklist records store information about the Checklist. The MI MOC Checklist family is also used in the MOC module to store information about the Checklist that are associated with a Change Project. This topic provides an alphabetical list and description of the fields that exist for the MI MOC Checklist family and appear on the MI MOC Checklist datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive, and contains only those fields that are used in the Application Settings for Management of Change.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Change Type | Character | The type of change for which the Checklist can be used. | You can enter a value manually. |
Checklist ID | Character | The identification for the Checklist. |
This field is required. You must enter a unique value in this field. On the datasheet, this field is labeled as Checklist. |
Description | Character | The description of the Checklist. | You can enter a value manually. |
Copyright © 2018 General Electric Company. All rights reserved.