MI MOC Answer Option Records

MI MOC Answer Option records store information about an Answer Option for a Question and the corresponding Exception that must be triggered for the Answer Option. The MI MOC Answer Option family is also used in the MOC module to store information about the Answer Options for Checklist Questions that are associated with a Checklist of a Change Project. This topic provides an alphabetical list and description of the fields that exist for the MI MOC Answer Option family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive, and contains only those fields that are used in the Application Settings for Management of Change.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Answer Character Identifies the response that triggers an Exception.

This field appears as a list that is populated by the MI_MOC_ANS_OPT System Code Table.

Exception ID Character The identification of the Exception that must be created on selection of the response indicated in the Answer field.

You can select the Exception that you want to associate with the Answer Option.

On the datasheet, this field is labeled as Exception Triggered.

Exception Key Numeric Contains the Entity Key of the Exception indicated in the Exception ID field. This field does not appear on the datasheet and is populated automatically.

Copyright © 2018 General Electric Company. All rights reserved.