Datalogger Mapping Records

Datalogger Mapping records are used to determine the relationship between fields in GE Digital APM families and fields used in a datalogger. This topic provides an alphabetical list and description of the fields that exist for the Datalogger Mapping family. The information in the table reflects the baseline state and behavior of these fields.

This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.

Field Data Type Description Behavior and Usage
Device Type Character The type of the datalogger whose field you want to map.

This field contains the description of all the System Codes in the M655 System Code Table. You can choose from the following baseline values:

  • GE DMS2
  • GE DMS Go/Go+
  • Olympus 37DL Plus Ultrasonic Thickness Gage
  • Olympus 37DL Plus Ultrasonic Thickness Gage
Source Family Character The name of the GE Digital APM family whose field you want to map as the source.

If the value in the Transfer Direction field is Send To (T), then this field contains the following list of families:

  • Thickness Measurement Location
  • TML Corrosion Analysis

If the value in the Transfer Direction field is Receive From (F), then this field contains the following list of families:

  • Thickness Measurement
  • Thickness Measurement Location
Source Field Character The name of the field that you want to map as the source. This field contains a list of fields in the family that you have selected in the Source Family field.
Target Field Character The name of the field that you want to map as the target.

This field contains a list of fields in the datalogger that you have selected in the Device Type field. It contains the description of the system Codes in the M658 System Code Table. You must only use the baseline fields that appear in this field.

By default, on the TM Dataloggers page, in the Send To and Receive From sections, the rows in the grids are arranged in the alphabetical order of the values in the Target Field column.

Transfer Direction Character Indicates whether data is sent to or received from the datalogger.

This field contains the description of all the System Codes in the M656 System Code Table. You can choose from the following baseline values:

  • Send To (T)
  • Receive From (F)

Copyright © 2018 General Electric Company. All rights reserved.