Super Users and members of the MI AHM Administrator Security Group can use the Event Mapping workspace to customize the information that is displayed in the Events section in Asset Health Manager. For more information about events, see the end user documentation for Asset Health Manager.
Boxes that you can use to specify a new event mapping appear.
In the Mapped Family box, select the family whose event information you want to appear in Asset Health Manager.
Note: The family that you select must:
Have a relationship to a family in the asset hierarchy.
Contain a date/time field that can be mapped to the Start Time Field.
In the Allow event consolidation? section, specify whether or not you want to allow events for this family to be consolidated.
Note: In order for events to be consolidated, the Has Consolidated Events relationship must also be configured for this family. Also, Asset Health Manager users who will perform event consolidation must belong to a Security Group that includes Insert and Update privileges on the family.
In the Event Relationship box, select the relationship family that links the asset to the source event record.
Note: For performance reasons, you cannot map long text fields to these fields.
In the Default Severity box, select the severity that should be associated with the source event record if the value in the specified Severity Field does not contain a specifically defined Mapped Severity Code.
Define event severities for specific values as necessary. To do so:
In Event Severities heading, select .
Boxes that you can use to specify a severity appear.
In the Select Severity code... box, select the type of severity you want to define.
In the Mapped Severity Code box, enter the value that corresponds to the selected severity.