Access the Event Mapping Workspace

Super Users and members of the MI AHM Administrator Security Group can use the Event Mapping workspace to customize the information that is displayed in the Events section in Asset Health Manager, as well as whether event records can be consolidated. For more information about events, see the end user documentation for Asset Health Manager.

Steps

  1. Access the Application Settings page.

  2. Select Asset Health Manager.

    The AHM Admin page appears, displaying the Event Mapping workspace.

    The family selected in the Mapped Family box indicates the family that is being mapped as a source event family.

    The Allow event consolidation? selection specifies whether or not you want to allow events for this family to be consolidated.

    Note: In order for events to be consolidated, the Has Consolidated Events relationship must also be configured for this family.

    The Event Fields section contains the following boxes:

    The Event Severities section specifies the severity that is associated with specific values in the specified Severity Field of the source event family. The severity is shown as an icon representing Information, Warning, or Alert in the Events section in Asset Health Manager.

Event Severity Example

For example, based on the event severity mappings shown in the preceding image, when the Severity field in a Policy Event record contains the value WRN, the Warning icon is displayed in the Events section of Asset Health Manager. If the Severity field in a Policy Event record contains a value other than INF, WRN, or ALT, the default severity will be used (i.e., Information).

Copyright © 2018 General Electric Company. All rights reserved.