Calibration Template, Single Component Analyzer Records

Calibration Template, Single Component Analyzer records store details on the single component analyzer calibration that should be performed for a specific piece of equipment. This topic provides an alphabetical list and description of the fields that exist for the Calibration Template, Single Component Analyzer family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field Name Data type Description Behavior and Usage
Asset Key Numeric The Entity Key of the Equipment that is linked to the Calibration Template.

This field does not appear on a datasheet by default. When you apply a Calibration Template to an Asset, the details of the Asset are retrieved based on the value in the Asset Key field.

This field is used by the GE Digital APM system and should not be modified.

Calibration Strategy Character The strategy for the single component analyzer calibration. This field contains a list of strategies for the analog calibration. This field is required. You can choose from the following strategies:

  • 2 Up

  • 2 Down

  • 2 Up then 2 Down

  • 3 Up

  • 3 Down

  • 3 Up then 3 Down

  • 5 Up

  • 5 Down

  • 5 Up then 5 Down

  • 5 Up then 1 Down

  • 11 Up

  • 11 Down

  • 11 Up then 11 Down

Depending on the selection on the Calibration Template Detail, Analyzer record, the following fields are populated by default:

  • Calibration Template Detail ID

  • Input Up/Dn
  • Percent of Scale Sequence Number

  • Percent of Scale Test Point

After you save the template, you cannot modify this field.

Calibration Task ID Character The ID of the Calibration Task that is linked to the Equipment to which the Calibration Template is linked. This list contains the IDs of the Calibration Tasks that are linked to the Equipment to which the Calibration Template is linked. You can select the desired Calibration Task from the list. If the Equipment is not linked to a Calibration Task, this list will be empty.
Calibration Type Character The type of calibration for which you are creating the template.

This field is disabled and populated with the value ANALYZER-SINGLE COMPONENT by default.

Input Type Character The input type for the single component analyzer calibration.

This field appears as a list that is populated by the MI CALIBRATION IO TYPES System Code Table. You can choose from the following input types:

  • Current
  • Resistance

  • Voltage

  • Pulse
  • Other

  • HART

This field is required.

Manufacturer Character The manufacturer of the Equipment that is linked to the Calibration Template. This field is disabled and populated with the value stored in the Manufacturer field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank.
Max Error Limit Numeric The maximum percentage of error that is allowed before a calibration event is considered failed. This field is populated with the value specified in the SC Analyzer Error Limit field in the Calibration Setup Defaults record. You can modify this value if required.
Model Number Character The model number of the Equipment that is linked to the Calibration Template. This field is disabled and populated with the value stored in the Model Number field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank.
Output Type Character The output type for the single component analyzer calibration.

This field appears as a list that is populated by the MI_CALIBRATION_IO_TYPES System Code Table. You can choose from the following output types:

  • Current
  • Resistance
  • Pulse
  • Observed
  • Voltage
  • Other
  • HART

This field is required.

Primary Input LRV Numeric A number representing the lower range value for the primary input range.

This field is grouped with the following other fields in the Primary Input Details section:

  • Primary Input URV
  • Primary Input Range Units

The value stored in the Primary Input LRV field combined with the value stored in the Primary Input URV field define the primary input range for the calibration. This field is required.

Primary Input Range Units Character The units of measure (UOM) for the primary input.

This field is grouped with the following other fields in the Primary Input Details section:

  • Primary Input LRV
  • Primary Input URV

This list contains a list of UOMs that is filtered based on the value in the Input Type field. This means that only the UOM values that are relevant for that input type will appear in the list. After you select a value in this list, the GE Digital APM system checks to see if the UOM is compatible with the device. If the selected values are not compatible, an error message will appear, indicating the problem.

Primary Input URV Numeric A number representing the upper range value for the primary input range.

This field is grouped with the following other fields in the Primary Input Details section:

  • Primary Input LRV
  • Primary Input Range Units

The value stored in the Primary Input URV field combined with the value stored in the Primary Input LRV field define the primary input range for the calibration. This field is required.

Primary Output LRV Numeric A number representing the upper range value for the primary output range.

This field is grouped with the following other fields in the Primary Output Details section:

  • Primary Output URV
  • Primary Output Range Units

The value stored in the Primary Output LRV field combined with the value stored in the Primary Output URV field define the primary output range for the calibration. This field is required.

Primary Output Range Units Character The units of measure (UOM) for the primary input.

This field is grouped with the following other fields in the Primary Output Range section:

  • Primary Output LRV
  • Primary Output URV

This field contains a list of UOMs that is filtered based on the value in the Output Type field. This means that only the UOM values that are relevant for that output type will appear in the list. This field appears as a list that is populated by the MI_CALIBRATION_IO_TYPES System Code Table. After you select a value in this list, the GE Digital APM system checks to see if the UOM is compatible with the device. If the selected values is not compatible, an error message will appear, indicating the problem.

Primary Output URV Numeric A number representing the upper range value for the primary output range.

This field is grouped with the following other fields in the Primary Output Details section:

  • Primary Output LRV
  • Primary Output Range Units

The value stored in the Primary Output URV field combined with the value stored in the Primary Output LRV field define the primary output range for the calibration. This field is required.

Refresh Equipment Data Boolean Indicates whether or not information in the Equipment that is linked to the Calibration Template has been updated. This field does not appear on the datasheet by default. This field is used by the GE Digital APM system and should not be modified.
Serial Number Character The serial number of the Equipment that is linked to the Calibration Template.

This field is disabled and populated with the value stored in the Serial Number field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank.

Tag Description Character The description of the piece of equipment, which is represented by the Equipment that is linked to the Calibration Template. This field is disabled and populated with the value stored in the Equipment Short Description field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank.
Tag Name Character The ID of the Equipment that is linked to the Calibration Template. This field is disabled and populated with the value in the Equipment field in the Equipment record that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank.
Template ID Character The ID of the template. This field is required and must be unique.
Template State Character The state of the Calibration Template.

This list contains the following values:

  • Development
  • Approved
  • Obsolete

The default value is Development.

Related Information

Copyright © 2018 General Electric Company. All rights reserved.