Calibration Template Detail, Analyzer

Calibration Template Detail, Analyzer records store information about the single component analyzer calibration strategy details. This topic provides an alphabetical list and description of the fields that exist for the Calibration Template Detail, Analyzer family and appear on the Calibration Template, Single Component Analyzer datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Calibration Template Detail ID Character The ID of the calibration template.

This field is populated automatically with the ID of the calibration template.

Component Name Character The name of the standard gas component.

This field is populated by the MI_CHEMICAL_COMPONENTS System Code Table.

You can enter a value manually.

Component Units Character The units of measure for the composition of the standard gas component.

You can enter a value manually.

Component Value Numeric A number representing the amount of gas in the cylinder.

You can enter a value manually.

Input Up/Dn Character

A value representing the up or down value range of a test point for a calibration strategy.

This field is populated automatically based on the value that you selected in the Calibration Strategy field.

Percent of Scale Sequence Number

Numeric

A number representing the sequence for the percentage of scale test points.

This field is populated automatically based on the value that you selected in the Calibration Strategy field.

Percent of Scale Test Point Numeric A number representing the percentage of test points. This field is populated automatically based on the value that you selected in the Calibration Strategy field.

Related Information

Copyright © 2018 General Electric Company. All rights reserved.