Calibration Template, Functional Test records store information about a functional test that should be performed on a piece of equipment. This topic provides an alphabetical list and description of the fields that exist for the Calibration Template, Functional Test family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field Name | Data Type | Description | Behavior and Usage |
---|---|---|---|
Calibration Task ID | Character | The ID of the Calibration Task that is linked to the Equipment to which the Calibration Template is linked. | This field contains the IDs of all the Calibration Tasks that are linked to the Equipment that is linked to the Calibration Template. You can select a Calibration Task from the list. If the Equipment is not linked to any Calibration Task, then this list will be empty. |
Calibration Type | Character | The type of calibration for which you are creating the template. |
This field is disabled. Based on the type of template that you selected on the Profile Template page, this field is populated with one of the following values:
|
Manufacturer | Character | The manufacturer of the Equipment that is linked to the Calibration Template. | This field is disabled and populated with the value stored in the Manufacturer field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank. |
Model Number | Character | The model number of the Equipment that is linked to the Calibration Template. | This field is disabled and populated with the value stored in the Model Number field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank. |
Serial Number | Character | The serial number of the Equipment that is linked to the Calibration Template. |
This field is disabled and populated with the value stored in the Serial Number field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank. |
Tag Description | Character | The description of the Equipment that is linked to the Calibration Template. | This field is disabled and populated with the value stored in the Equipment Short Description field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank. |
Tag Name | Character | The ID of the Equipment that is linked to the Calibration Template. | This field is disabled and populated with the value in the Equipment field in the Equipment record that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank. |
Template ID | Character | The ID of the Calibration. |
This field is required and must be unique. |
Template State | Character | The state of the Calibration Template. By default, this field contains the value Development. |
This list contains the following values:
You can select a value in this list. |
Copyright © 2018 General Electric Company. All rights reserved.