Calibration Template Detail, Functional Test Records

Calibration Template Detail, Functional Test records store information about a functional test that should be performed on a piece of equipment. This topic provides an alphabetical list and description of the fields that exist for the Calibration Template Detail, Functional Test family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field Name Data Type Description Behavior and Usage
Condition Character A possible answer to an instruction that has the response type list. You can define up to 10 conditions (i.e., options) for each list response type. This field is enabled only if the value stored in the Response Type field is List.
Instruction Text The step you are performing during the functional test (e.g., Describe the condition of the wires). None
Response Type Character The type of response you should give to the question defined in the Instruction field.

This field appears as a list that is populated by the MI_CALIBRATION_CHECKLIST_TYPE System Code Table. You can select one of the following values:

  • Yes/No: The response will be either Yes or No.
  • Number: The response will be a numeric value.
  • Text: The response will be a text value.
  • Selection: The response will be one or more of the options provided in the Condition fields.
Sequence Number Numeric A numeric value that represents the order in which the step identified in the Instruction field should be executed in relation to the other steps. This list contains numeric values from 1 to 25. We recommend that you select values in sequential order (e.g., select the value 1 in the first record, select the value 2 in the second record), but if you do not, when you save the records, they will be sorted automatically according to the values stored in the Sequence Number fields. This field is required.

Related Information

Copyright © 2018 General Electric Company. All rights reserved.