The inventory component mass of a component is calculated using the values in the following fields in the Criticality Calculator RBI Component record:
Length (L)
Note: If the component type is Piping, then the value in the Piping Length field is used instead of the value in the Length field.
Note: If the component is linked to an RBI 581 Risk Analysis, then these values are taken from the corresponding fields in the analysis record instead of the component record.
The inventory component mass of a component is calculated as follows:
Inventory Component Mass = (Liquid Volume x Fluid Density) + (Vapor Volume x Vapor Density)
where:
Liquid Volume = (pc/100) x Volume of the cylinder
Note: The volume of the cylinder is calculated from the values in the Diameter and Length fields in the Criticality Calculator RBI Component record.
This value is populated in the Inventory Component Mass field in the Common section of the associated RBI 581 Consequence Evaluation.
Example for Calculating Inventory Component Mass
Suppose a component has the following specifications:
Component Type: Heat Exchanger (Shell)
Process Fluid : C6-C8
Operating Pressure: 101 Pounds/Sq Inch Gage
Operating Temperature: 121 Degrees Fahrenheit
Molwt of CO: 28
Diameter: 97.625 inches
Length: 360 inches
Percent Liquid Volume: 50 percent
Fluid Density: 42.704
Given these values:
Volume of the cylinder = (pi x (d/12) x (d/12) x (L/12)) / 4
Volume of the cylinder = ((22/7) x (97.625/12) x (97.625/12) x (360/12)) / 4
Volume of the cylinder = 1560.075 Cubic feet
Liquid volume = (pc/100) x Volume of the cylinder
Liquid volume = (50/100) x 1560.075
Liquid volume = 780.038 Cubic feet
Vapor volume = (1 - (pc/100)) x volume of the cylinder
Vapor volume = (1 - (50/100)) x 1560.075
Vapor volume = 780.038 Cubic feet
Vapor Density = (Molwt x (P + 14.7)) / (10.73 x (T + 459.15) x z)
Vapor Density = (100 x (101 + 14.7)) / (10.73 x (121 + 459.15) x 1)
Vapor Density = 1.859 Pounds per cubic feet
Inventory Component Mass = (Liquid Volume x Fluid Density) + (Vapor Volume x Vapor Density)
Inventory Component Mass = (780.038 x 42.704) + (780.038 x 1.859)
Inventory Component Mass = 34760.526 Pounds
Note: The value in the Inventory Component Mass field on the RBI Component datasheet may slightly differ from the value that is shown in the example. This happens because of rounding off some of the values.
Copyright © 2018 General Electric Company. All rights reserved.