Create a Custom Degradation Mechanism Evaluation (DME) Validation

Steps

  1. Access the Custom RBI Methodology Preferences workspace.

  2. Select the Custom DME Validation tab.

    The Custom DME Validation section appears.

  3. In the upper-right corner of the section, select .

    A new Custom DME Validation datasheet appears, displaying the Master section.

  4. Enter the following information:

    Tip: All required information is provided, however, for additional information, refer to the RBI Custom DME Evaluation Configuration records topic.

  5. Select the Detail tab.

    The Detail section of the Custom DME Validation datasheet appears.

  6. Enter the following information:

    Tip: All required information is provided, however, for additional information, refer to the RBI Custom DME Evaluation Configuration records topic.

  7. In the upper-right corner of the datasheet, select .

    The Custom DME Validation is created.

Results

Copyright © 2018 General Electric Company. All rights reserved.