RBI Custom DME Evaluation Methodology records store the configuration details for custom calculations and validations. This topic provides an alphabetical list and description of the fields that exist for the following families and their corresponding datasheets:
RBI Custom DM Validation Configuration Details
The information in the table reflects the baseline state and behavior of these fields.
These families are enabled for site filtering, which means that records in these families can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
RBI Custom DM Evaluation Configuration and RBI Custom DM Validation Configuration | |||
Analysis Family | Character | A list of available families that support Custom RBI Methodology Preferences. | By default, this field is populated with the value RBI Criticality Analysis. You cannot modify this value. |
Degradation Mechanism Evaluation Methodology | Character | The family ID of the Damage Mechanism Evaluation (DME) that will use the custom calculation. | A value is required. This field contains a list of all DME families that are configured with the Has RBI Degradation Mechanism Evaluation relationship definition that are not currently linked to the baseline GE Digital APM families. |
Output Fields | Boolean | A list of the field IDs that should be treated as output fields. | When an analysis containing the DME is copied, the selected output fields are not copied to the new DME. |
Policy Name | Character | The name of the policy used for custom calculation. | A value is required. This field contains a list of all policies in the MI_POLICY family. This policy updates the DME Entity. |
Sequence | Numeric | Defines the order in which the policies associated with this DME methodology should be fired. |
The value in this field must be a numeric value greater than 1. |
RBI Custom DM Evaluation Configuration Details and RBI Custom DM Validation Configuration Details | |||
Input Entity Family | Character | The family of the Entity type of the policy that creates the custom DME. The value in this field will be from the RBI Custom DME Evaluation Configuration family. |
This field contains a list of:
|
Policy Node Name | Character | The name of the node in the policy to which the Entity is mapped. | A value is required. |
Copyright © 2018 General Electric Company. All rights reserved.