As you navigate through the Asset Hierarchy, at each level, information about the Health, Reliability, Strategy, and Integrity of that level is displayed on the <Asset Name> page. The <Asset Name> page provides a snapshot of all the data in GE Digital APM related to the asset selected in the Asset Hierarchy. For each Health, Reliability, Strategy and Integrity item, there is a hyperlink displaying the number and type of analysis performed against that asset. The hyperlinks, once selected, open the analyses or inspections in a new tab while maintaining the selection in the Asset Hierarchy.
Example: View an Asset Criticality Analysis from an asset in the Asset Hierarchy
To view the ACAs for the Area Meridium Roanoke Refining:
-
Navigate to the Area Meridium Roanoke Refining.
Meridium Roanoke Refining is selected in the Asset Hierarchy, the Meridium Roanoke Refining page is displayed, and the Health tab is selected. From this page, you can view the Risk snapshot e.g. there are 4 Active AMS Alerts, 10 ACAs, 184 Health Indicators, 11 Calibration Tasks, etc. against the asset, as shown in the following image.
-
Select the 10 ACA Analyses link.
The ACA Overview page opens in a new tab, and the selection in the Asset Hierarchy, Meridium Roanoke Refining, is displayed under Asset Criticality Analysis, as shown in the following image.