To create the Task record, make sure to use the Task Builder and not the Record Manager. Otherwise, the Task record will not be linked to the Equipment or Functional Location record, and the Work Management Adapter will not work as expected.
You can create an SAP Order from a Task record only if all of the following conditions are true:
Steps
In the Task record, in the Task List field, select
The Locate Task List window appears.
In the Search Criteria section, enter the desired search criteria.
Note: If you accept the default criteria, the search results will return all Task Lists.
Select Search.
The Task Lists that meet the search criteria appear in the Search Results section.
In the Search Results section, select the row containing the desired Task List, and then select OK.
The Task List field on the Task record is updated with the Task List group number.
In the Desired Interval field, enter the desired interval.
The value in the Next Date field is updated automatically based on the Last Date and the Desired Interval.
In the Call Horizon field, enter the desired call horizon.
Tip: For details about call horizons, see the SAP Help, which is located at http://help.sap.com/.
Save the Task record.
Copyright © 2018 General Electric Company. All rights reserved.