Install SAP Java Connector

To facilitate the data transfer, there must be a java connector between SAP and the APM Connect server. This topic describes how to establish the connection via the SAP Java Connector (SAP JCO).

Note: The APM Connect installer automatically places the files sapjco3.dll and sapjco.jar into the location C:\APMConnect\Utilities\runtime\lib. You must complete the remaining steps in this topic manually.

Steps

  1. Navigate to the location where you downloaded the SAP Java Connector package from the SAP marketplace, and copy the following files:

    Note: If you are using a 64-bit machine, per the APM Connect system requirements, you must select the 64-bit installer.

  2. Navigate to C:\APMConnect\Utilities\runtime\lib\wrapper, and then paste the copied files in that location.
  3. Copy the file sapjco3.dll again.
  4. Navigate C:\windows\system32, and then paste the copied file in that location.

    The Java Connecter is installed.

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.