Sample BackupRestore.ini

Use the BackupRestore.ini to specify default and custom settings that appear in the Backup and Restore Wizard, and when you run BackupRestore.exe from a command line. The BackupRestore.ini file is located in the iFIX LOCAL folder. If you installed iFIX to the default location, you can find the BackupRestore.ini in the C:\Program Files (x86)\GE\iFIX\LOCAL folder.

The BackupRestore.ini file can contain information in the following sections:

  • [Version] – used to determine iFIX product version in archive header signature. This section is required. Do not change this value.
  • [DefaultSubProject] – used to determine default sub-project paths for the Create New Project option in the Restore operation.
  • [FactoryDefaultExtension] – used to determine which files are included in Factory Default settings.
  • [WizardSettings] – used to determine file name and path (if it is different than your iFIX base path) of the Factory Default file when you select the "Restore default iFIX files before restoring your backup files" option during a Restore operation.
  • [AddCustomExtension] – used if you want to include or exclude any additional files or file types in your custom backup. By default, the AddExtension feature is set to False. Set AddExtension to True to enable this feature. Each category has keys to include (xxxIncludeExtn=) and exclude (xxxxExcludeExtn=) files. The xxxxExcludeExtn key is used to exclude files from xxxxIncludeExtn key, not to exclude a default extension.

The entire key can be up to 2048 characters long, in total. If you exceed this length, for instance if the path is too long, an error message appears and the custom file or file extension is ignored when you attempt the backup.

IMPORTANT: Make sure that you do not include the same file or file extension (from the same location) in more than one category.  If you back up the same file or file type in more than one category, you will experience issues restoring your files. Configure your custom settings carefully.

By default, the Backup and Restore application references the BackupRestore.ini file when it runs. If you want to change the name of the .INI file, you must run BackupRestore.exe with the /i command line option, and specify the file name of the custom .INI file. If you create a custom .INI file, it must follow the same format described above.

The following is an example of the BackupRestore.ini from the iFIX LOCAL folder that includes all four of the sections defined above:

;BackupRestore.ini - Customizing your BackupRestore.ini file

;

;[Version]

; Do not change the Version key.

; If you create your own .ini file using the /I option, this section and key are required.

;

;[DefaultSubProject]

; 1. If you select the "Create New Project" destination option,

; define the sub-project folders here.

; 2. If you use the /P option during backup, the sub-project folders defined here are archived.

; 3. If you use the /P option during restore, the archive files are restored to the sub-project

; folders defined here.

;

;[FactoryDefaultExtension]

; If you generate your own FactoryDefault file, use this section to define which files to

; include in your FactoryDefault backup.

;

;[WizardSettings]

; Use the FACTORYDEFAULT key in your FactoryDefault file when select the "Restore default

; iFIX files before restoring your backup files" option during a restore.

;

; The FACTORYDEFAULT_PATH key is used for your FactoryDefault file path. If this section is blank,

; your current BASEPATH is used.

; For example: FACTORYDEFAULT_PATH=C:\MySetting (do not add "\" at the end)

;

;[AddCustomExtension]

; If you like to add file type to custom backup, it allows you to define

; additional extension for each categories to include/exclude files to backup.

; To make it enabled, change AddExtension to True.

; AddExtension=TRUE

; Then, add file name or file type for specific key in categories. For example:

; [AddCustomExtension]

; AddExtension=TRUE

; PicIncludeExtn=*.bmp,*.jpg

; PicExcludeExtn=aaaa.bmp

;

[Version]

Version=6.50

[DefaultSubProject]

LOCPATH=LOCAL

PDBPATH=PDB

NLSPATH=NLS

PICPATH=PIC

APPPATH=APP

HTCPATH=HTR

HTDPATH=HTRDATA

HTRDATA=HTRDATA

ALMPATH=ALM

RCMPATH=RCM

RCCPATH=RCC

AADPPATH=PDB

AADBPATH=PDB

ADDONPATH=ADDON

[FactoryDefaultExtension]

ALM_EXTN=*.*

APP_EXTN=*.grf,*.tbx,sqlerr.txt

HTR_EXTN=*.csv

HTRDATA_EXTN=*.*

LOCAL_EXTN=*.json,CONFIGDB\*.json,UA\*.*,iFIX_OpcuaConfigService\*.pfx,OpcUaDefinitions.csv,Serverconfig.xml,Association.dat,RibbonAssociation.dat,default.fmt,FindReplace.csv,SystemTree.csv,default.qry,default.rft,default.srt,logmsg.tov,StandardCategories.txt,*.tbc,*.tbx,*.xbt,*.ico,*.bmp,*.ini,ImportToolbars.txt,autoStartKey.dat

PDB_EXTN=CGW.csv,Default.SM2,empty.pdb,*.tbl,iFixUaClient\*.json,*.json

PIC_EXTN=WizLayouts.tpl,*.fds,*.ftb,*.fxg,*.grf,*.SBL,*.BDF,*.odt,*.SVA,*.VGA,*.kmx,*.CSV,TS.ini

RCC_EXTN=*.*

RCM_EXTN=*.*

ADDON_EXTN=*.ini,*.tbc

[WizardSettings]

FACTORYDEFAULT=FactoryDefault.IFD

FACTORYDEFAULT_PATH=

;

; Custom extension

;

[AddCustomExtension]

AddExtension=FALSE

;

;Configuration files (*.SCU,*.INI,*.CFG), LOCPATH

SCUIncludeExtn=

SCUExcludeExtn=

;

;Picture files (*.GRF,*.FDS,*.FTB,*.LST), PICPATH

PicIncludeExtn=

PicExcludeExtn=

;

;Database files (*.PDB,*.AAD), PDBPATH

PDBIncludeExtn=

PDBExcludeExtn=

;

;Database ASCII files (*.GDB), PDBPATH

GDBIncludeExtn=

GDBExcludeExtn=

;

;Driver Configuration Binary files (*.*), PDBPATH

DrvIncludeExtn=

DrvExcludeExtn=

;

;Database/Driver CSV files (*.CSV), PDBPATH

DBCSVIncludeExtn=

DBCSVExcludeExtn=

;

;Historical Config files (.CFG,*.HGP,*.DAT), HTCPATH

HistConfigIncludeExtn=

HistCOnfigExcludeExtn=

;

;Tag Group files (*.TGD,*.TGS,*.TGE), PICPATH

TagGroupIncludeExtn=

TagGroupExcludeExtn=

;

;Recipe Control files (*.RCC,*.RCY), RCCPATH

RCPIncludeExtn=

RCPExcludeExtn=

;

;Master Recipe files (*.RCM,*.RCX), RCMPATH

RCMIncludeExtn=

RCMExcludeExtn=

;

;Application files (*.*), APPPATH

APPIncludeExtn=

APPExcludeExtn=

;

;Project Toolbar files(*.TBX,*.TBC), LOCPATH

ToolbarIncludeExtn=

ToolbarExcludeExtn=

;

;Event Schedule files (*.EVS), PDBPATH

ScheduleIncludeExtn=

ScheduleExcludeExtn=

;

;Project Global Definition Files(*.FXG), PICPATH

FXGIncludeExtn=

FXGExcludeExtn=

;

;Chart Group Wizard files(*.CSV), HTCPATH

CGWIncludeExtn=

CGWExcludeExtn=

;

;FIX32 Picture files(*.ODF,*.ODT,*.SBL), PICPATH

FIX32PicIncludeExtn=

FIX32PicExcludeExtn=

;

;FIX32 KeyMacro files(*.KMX), PICPATH

Fix32KMEIncludeExtn=

Fix32KMEExcludeExtn=

;

;Addon files(*.INI,*.TBC), ADDONPATH

AddonIncludeExtn=

AddonExcludeExtn=

;

 

See Also