Starting iFIX with an SCU File from a Different Path

To start iFIX with an SCU file from a different path:

NOTE: The following steps describe how to modify an SCU file with a path outside the install path, so that you run it in iFIX.

  1. Shut down iFIX.
  2. On the Start menu, point to Programs, iFIX, and then System Configuration to open the SCU. The SCU window appears.
  3. From the SCU Configure menu, click Paths. The Path Configuration dialog box appears.
  4. In the Path Configuration dialog box, change the base path and NLS path to point to the local install path. Change the project path to point to the project destination folder, if it does not already do so.
  5. From the SCU Configure menu, click Tasks. The Task Configuration dialog box appears.
  6. In the Task Configuration dialog box, change the path of the configured tasks to the local install path, make sure that you include the same command line options.
  7. From the SCU Configure menu, click Network. The Network Configuration dialog box appears.
  8. In the Network Configuration dialog box, confirm the information is correct and make changes if necessary.
  9. From the SCU Configure menu, click SQL, and then click Configure SQL Tasks. The SQL Task Configuration dialog box appears.
  10. In the SQL Task Configuration dialog box, make sure that the Primary and Secondary paths are correct, if used.
  11. From the SCU Configure menu, click Local Startup. The Local Startup Definition dialog box appears.
  12. In the Local Startup Definition dialog box, change the path to the folder you copied the project to with the get command.
  13. From the SCU File menu, click Save.
  14. Restart iFIX.

See Also