Changing the Plotting Color and Style of an Enhanced Chart

To change the plotting color and style of an enhanced chart:

  1. In the iFIX WorkSpace picture, double-click the chart. The Enhanced Chart Customization dialog box appears.
  2. Click the Plotting Style tab and in the Line Style area, click the desired color. To create a custom color, double-click a color.

NOTE: The selected color is applied to the X and Y axis markers, Data Sources table items, and graph lines and points.

  1. Line Charts Only: In the Chart Plotting Style area, select the desired style.
  2. Line Charts Only: Select a Point Type.

NOTE: Point types appear only if the Chart Plotting Style includes points, such as Point + Line, for example.

  1. Select a Line Type.
  2. In the Data Shadows area, click Off, Shadow, or 3D.

NOTE: 3D can be applied only to Histograms; Shadow can be applied to only Histograms and Line/Multiline charts that use Area or Bar for their Plotting Style.

  1. Click OK.

See Also