I/O Drivers Folder

From the I/O Drivers folder you can manage:

  • Binary I/O Driver Configuration Files (*.yyy, where yyy is the driver acronym).
  • IGS Driver files (*.OPF).

IMPORTANT:

  • To manage driver configuration files, you must add the driver in the SCU's SCADA Configuration dialog box. To add the I/O driver from the SCU, in the Configure menu, click SCADA. In the I/O Driver Definition area, click the browse (...) button to select the I/O driver name, and then click Add.
  • Be aware that configuration files for 7.x series drivers saved outside of the iFIX database directory cannot be managed from the integrated iFIX with Change Management environment. If you installed iFIX to the default location, the path to the iFIX database directory is: C:\Program Files (x86)\GE\iFIX\PDB.

See Also