Selecting Tables in an SQL UPDATE Command
To select tables
in an SQL UPDATE command using the SQL Wizard:
- Run the SQL Wizard and on the Select Operation dialog box, click SQL Update.
- Proceed in the SQL Wizard until you reach the Select Table To Update dialog box.
- In the Select Table To Update dialog box's Available Tables list, select a table and click Add. Repeat this action for each table required for the SQL statement or, to add all the tables, click All >>.
- To re-order the sequence of selected tables, select a table in the Selected Tables list and click the Up or Down arrow to move the table up or down in the list.
- Click Next to continue creating the query.
- Or -
Click Back to return to the previous screen in the SQL Wizard.
- Or -
Click Finish if the query is done.
NOTE: To remove a table from the statement, select it from the Selected Tables list and click Remove All to remove all the tables in the statement.
See Also