Select Operation Dialog Box
The Select Operation dialog box contains the following buttons:
SQL SELECT
Select this option to construct a SQL SELECT command. For more information on the dialog boxes associated with the SQL SELECT command construction, see SQL SELECT Dialog Boxes.
SQL INSERT
Select this option to construct a SQL INSERT command. For more information on the dialog boxes associated with the SQL INSERT command construction, see SQL INSERT Dialog Boxes.
SQL UPDATE
Select this option to construct a SQL UPDATE command. For more information on the dialog boxes associated with the SQL UPDATE command construction, see SQL UPDATE Dialog Boxes.