To set the statistics refresh
rates:
- From the Options menu, choose Setup. The Setup dialog box appears.
- Select the Display Setup tab.
- In the Server/Group Dialog field, enter the refresh rate for the server and group levels.
- In the Item Dialog field, enter the refresh rate for the item level.
Valid refresh rates for the Item and Server/Group levels are between 1000 and 60000. Valid refresh rates for the Secondary rate are between 5000 and 360000.
- In the Secondary Rate field, enter the secondary refresh rate.
The secondary refresh rate is used if an error is received from the server. The primary (server/group or item) refresh rate is ignored and the refresh rate entered in this field is used.
NOTE: System and channel (Server) statistics have a different update rate than the datablock (Item) because the statistics at the server level do not change as often as at the item level.
See Also