Click the following links for detailed process information:
- Add the OPC Client to a SCADA configuration and launching the Power Tool
- Configure a group with the Power Tool
- Add a link to a picture that accesses the group
You can set up a single Data link and enable communications between iFIX and the process hardware with the OPC Client.
You must configure a group in the I/O Driver Power Tool first, then open a picture in the iFIX WorkSpace and set up a data link that accesses process hardware using the OPC Client. When you enter the I/O address, the item is automatically be created and the I/O Server starts polling for data.
To add the
OPC Client to a SCADA configuration and launch the Power Tool:
- Start the System Configuration Utility (SCU):
From the Start menu, point to Programs, then iFIX and click System Configuration from the menu that appears.
- From the Configure menu, choose SCADA.
- Click the question mark (?) next to the I/O Driver Name box. A list of drivers installed on the local node appears.
- Select the OPC Client and click Add. The SCU adds the OPC Client to the Configured I/O Drivers list.
- Save and exit the SCU.
- Start or restart iFIX.
- Start the OPC Power Tool:
From the Start menu, point to Programs, then iFIX and click OPC Power Tool.
To configure
a group with the Power Tool:
- Add a Server to the Power Tool.
- On the Server Properties Viewer, select the Enable check box.
- From the Display Mode menu, choose Stats Mode to verify that the driver is connected to the OPC server. The Power Tool displays statistics for the selected server.
- From the Display Mode menu, choose Config Mode to display the server’s properties.
- From the Edit menu, choose Add Group. The Power Tool adds a group to the Tree Browser, under the selected server.
- In the Properties Viewer, enter the appropriate information for the group and a unique name for the group.
To add an
iFIX picture that accesses the configured group:
- From the OPC Client Power Tool Options menu, choose Setup. The Setup dialog box appears.
- Click the Advanced tab and choose Auto Create On from the Server area.
- Start the iFIX WorkSpace.
- For detailed information on adding a datalink in an iFIX Picture, see the Adding DataLinks topic in the Creating Pictures e-book.
- From the iFIX WorkSpace:
- In Ribbon view, on the Home tab, in the WorkSpace group, click Switch to Run.
- Or -
- In Classic view, on the WorkSpace menu, choose Switch to Run.
This action activates the run-time environment. Data from the hardware appears in the link. If it does not, refer to the Troubleshooting section.
See Also