To troubleshoot automatic driver
startup:
- Make sure the driver is installed in your root iFIX or Dynamics directory. If you have not installed the driver in this directory, uninstall it and then re-install it in the proper path.
- Next, start the Power Tool and verify that it is configured correctly:
- Verify that the servers, groups, and items are enabled.
- Make sure the Auto Start option is turned on:
- From the Options menu, choose Setup. The Setup dialog box appears.
- Click the Advanced tab.
- From the I/O Server area, click the Auto Start On option button.
- Specify a default path and configuration file name for the driver:
- From the Options menu, choose Setup. The Setup dialog box appears.
- Click the Default Path tab.
- Enter the configuration file’s default name and default path in the fields provided.
- Finally, start the System Configuration Utility (SCU) and verify it is configured correctly:
- Click the SCADA button from the SCU toolbox. You should see the following text in the dialog box that appears:
OPC - OPC Client vX.XX
- If you do not see this text, Select the ? button next to the I/O Driver Name.
- Select the OPC Client from the dialog box and click OK.
- Click Add to add the selected I/O driver to the Configured I/O Drivers list box.
- Click OK again to close the SCADA Configuration dialog box.
- Select Tasks from the Configure menu. When the Task Configuration dialog box appears, you should see IOCNTRL.EXE /a listed in the Configured Tasks list box.
- If you do not see this text, enter the Base path and IOCNTRL.EXE /a in the Filename field.
- Click OK to save your changes and save your SCU configuration.
- Restart iFIX. The driver should automatically start.
See Also