To change the
options for the Application Validator:
- In the iFIX WorkSpace, double-click Application Validator in the system tree. The Application Validator opens.
- On the Tools menu, click Options. The Application Validator Options dialog box appears.
- From the Exclusion List tab, enter the files that you want to exclude from the comparison. For each entry:
- In the edit box, enter the file name or file mask. For file name masks, you can use standard Windows wildcard characters. For instance, use the * symbol to represent multiple unknown characters in a file name. Use the ? symbol for a single unknown character in a file name.
- Click Add to add the file or file name mask to the file exclusion list.
- For example, if you do not want to include log files in your comparison, you would add *.log to the file exclusion list.
NOTE: Do not include the path information with the file name. For example, c:\*.log is not a valid entry in the exclusion list.
- Select the Application Execution tab. To define an application to run if differences are found when running the Application Validator from the command line:
- Select the Enable Application Execution check box.
- In the Application edit box, enter the location and name of the file. Optionally, click the Browse (…) button to search for a file.
- Select the Auto Report Naming tab. To use an automatic report naming convention when running the Application Validator from the command line:
- Select the Enable Auto Report Naming check box.
- In the Directory field, enter the location where you want to save the automatically created report. Optionally, click the Browse (…) button to locate and select a folder.
- In the Prefix field, enter the name you want to use for the report file. If you select the Auto Increment option, a number is added to the end of this name each time a new report is run from the command line.
- If you want to individually number each report file, instead of overwriting the original file each time you run a new report, select the Auto Increment check box.
- Click OK.