Application Validator Options Dialog Box
The Application Validator Options Dialog Box consists of three tabs:
Exclusion List Tab
Item |
Description |
Exclusion List |
Displays the files excluded when you compare the folders with the baseline. |
Excluded File Filter |
Enter the file or file name mask that you want to exclude from the folder comparison. Click Add to add it to the file exclusion list. For file name masks, you can use standard Windows wildcard characters. For instance, use the * symbol to represent multiple unknown characters in a file name. Use the ? symbol for a single unknown character in a file name. For example, if you did not want to compare log files versions you would add *.log to the file exclusion list. |
Exclusion List Text Box |
Enter the file or file name mask that you want to exclude from the folder comparison. Click Add to add it to the file exclusion list. For file name masks, you can use standard Windows wildcard characters. For instance, use the * symbol to represent multiple unknown characters in a file name. Use the ? symbol for a single unknown character in a file name. For example, if you did not want to compare log files versions you would add *.log to the file exclusion list |
Add |
Click to add the file or file name mask, entered in the field above, to the file exclusion list. |
Remove |
Click to delete the selected file or file mask from the file exclusion list. |
Application Execution Tab
Field Name |
Description |
Enable Application Execution |
Select this check box if you want to run an executable file when differences are found between the baseline and the current folder versions, when running the Application Validator from the command line. |
Application |
Enter the name and location of the file that you want to run (when the Application Validator runs from the command line) and finds differences. |
Browse |
Click to browse for a file. |
Auto Report Naming Tab
Field Name |
Description |
Enable Auto Report Naming |
Select this check box if you want to use a predefined name for all reports generated from the command line with the Application Validator. |
Report Name |
Enter the name for the auto-generated report file. If you select the Auto Increment option, a number is added to the end of this name each time a new report is run from the command line. |
Directory |
Enter the name and location of the folder to which you want to save the detailed summary reports generated when you run the Application Validator from the command line. |
Browse (...) |
Click to browse for a folder to which you want to save the report. |
Prefix |
Enter the name for the auto-generated report file. If you select the Auto Increment option, a number is added to the end of this name each time a new report is run from the command line. |
Auto Increment |
Select this check box if you want to individually number each report file, instead of overwriting the original file each time you run a new report. |