Thumbnail Property

When the Thumbnail property is set to True in an Enhanced Chart, the chart can be reduced in size and still show useful information. By reducing the size of the chart to a smaller size, multiple charts can be displayed in the same picture.

Syntax

object.Thumbnail [= Boolean]

Properties

The Thumbnail property syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

Boolean

Sets Thumbnail property to either True or False.

Settings

The settings for Boolean are:

Value

Description

True

The ShowYAxis, ShowXAxis, ShowTimeCursor, ShowLegend, ForceVerticalPoints, ShowDSLegend, and ShowTimeCursorTooltips will be set to the values listed in the following table. These values override any previously configured values for these properties.

False

All properties in following table are rendered to whatever you configure them to. (Default)

The following properties will be set to the values outlined in this table when the Thumbnail property is set to TRUE.

Property

Value when the Thumbnail Property is TRUE

ShowYAxis

Grid_only (3).

ShowXAxis

Grid_only (3).

ShowTimeCursor

FALSE.

ShowLegend

FALSE.

ForceVerticalPoints

PointLabelVertical (1).

ShowDSLegend

TRUE, if the data source legend is being displayed. However, only the Value column will appear.

ShowTimeCursorTooltips

FALSE.

 

Applies To