SeverityIncreased Event

Occurs when an alarm's status increases in severity. The CheckForSeverityIncrease property must set to TRUE to allow this event to be triggered. The CheckForSeverityIncrease property must be set in run mode. The value you enter here is not persisted. In other words, when you switch from run mode to configure mode, the value changes back to FALSE (0), which is the default. If you enter TRUE (1) in configure mode, it switches back to FALSE (0) when you enter run mode. You must set this value in run mode.

Syntax

object_SeverityIncreased( )

Properties

The SeverityIncreased event syntax has this part:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

 

Applies To