CheckForSeverityIncrease Property

Specifies whether the Alarm Summary object tracks when an alarm's status increases in severity and fires the SeverityIncreased event.

The CheckForSeverityIncrease property must be set in run mode. The value you enter here is not persisted. In other words, when you switch from run mode to configure mode, the value changes back to FALSE (0), which is the default. If you enter TRUE (1) in configure mode, it switches back to FALSE (0) when you enter run mode. You must set this value in run mode.

Syntax

object.CheckForSeverityIncrease [= Boolean]

Properties

The CheckForSeverityIncrease property syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

Boolean

Specifies whether the Alarm Summary object tracks when an alarm's status increases in severity and fires the SeverityIncreased event.

Settings

The settings for Boolean are:

Value

Description

True

Tracks changes to the list of alarms so that the SeverityIncreased event fires.

False

Does not track changes to the list of alarms. Consequently, the SeverityIncreased event never fires. (Default)

Remarks

The best place to set this property is in the Initialize event handler of your picture.

 

Applies To