SetPointAt Method

Modifies the location of the point at the given index to location specified.

Syntax

object.SetPointAt lIndex, pdispPoint

Properties

The SetPointAt method syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

lIndex

Long. The position of the point to modify.

pdispPoint

Object. The position to which to move the point.

Remarks

A point is an OLE object specifying a point object to add to the list of existing data points. The point object has an (x, y) pair that contains the coordinate of the data point (see FixFloatPoint.)

 

Example

Applies To