Selects a row in the Alarm Summary object.
Syntax
object.SelectAlarmRow(RowNum As Integer, bSelect As Boolean) As Integer
Properties
The SelectAlarmRow method syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
RowNum |
Integer. The row in the Alarm Summary object's spreadsheet you want to select. Row numbers start at 1 and you can specify any row even if it is not visible on the screen. |
bSelect |
Boolean. When True, the row is selected. When False, the row is not selected. |
Return Value
Zero. Reserved for future use.
Remarks
Selecting a row that is not displayed on the screen does not cause the spreadsheet to scroll to the selected row.
If you select a row that is not visible, you will not receive the Acknowledgement status, the Latched Alarm status, the Value, and the User Defined Columns when calling the GetSelectedRow or GetSelectedUserDefFields methods. You can work around this by reading these values after calling the GetSelectedRow method.