GetSelectedRow Method

Returns the information for the selected alarm in the Alarm Summary object. Note that even if a column is not displayed, all information is still returned.

Syntax

object.GetSelectedRow(bAcknowledged, Handle, Area, DateIn, DateLast, TimeIn, TimeLast, Node, TagName, Priority, Status, Description, Value, ExtField1, ExtField2, UserDefField1, UserDefField2)

Properties

The GetSelectedRow method syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

bAcknowledged

Boolean. Returns True if the alarm has been acknowledged, False otherwise.

Handle

String. Returns the unique identifier for the alarm. Specifically <type><ipn><nodename>.

Area

String. Returns the alarm area(s) for the alarm.

DateIn

String. Returns the date when the block first generated the alarm.

DateLast

String. Returns the date when the block last generated the alarm.

TimeIn

String. Returns the time when the block first generated the alarm.

TimeLast

String. Returns the time when the block last generated the alarm.

Node

String. Returns the name of the Scada server that generated the alarm.

TagName

String. Returns the tagname for the alarm.

Priority

String. Returns the priority for the alarm.

Status

String. Returns the latched alarm for the block that is in alarm.

Description

String. Returns the description field for the block in alarm.

Value

String. Returns the current value of the block in alarm.

ExtField1

String. Returns the first extension field for the block in alarm.

ExtField2

String. Returns the second extension field for the block in alarm.

UserDefField1

String. Returns the current value of the first "A_" field configured for this column.

UserDefField2

String. Returns the current value of the second "A_" field configured for this column.

Return Value

Boolean. True if an alarm is selected, False if no alarm is selected.

Remarks

If no alarm is selected, all parameters are set to EMPTY.

 

Example

Applies To