GetUserID Method

Returns the user ID (short name) from iFIX security for the given user name and password. This ID is used when sending a signed operator message.

Syntax

object.GetUserID(bstrUserName, bstrPassword, bstrUserID)

Properties

The GetUserID method syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

bstrUserName

String. The name of the event.

bstrPassword

String. The code to be written to the event in the form of strings.

bstrUserID

String. Returns the user ID (short name) of the user in iFIX security.

Return Value

This method returns HRESULT. If the HRESULT is a value other than S_OK, VBA generates an error. You can handle this error using the On Error Statement You can find out more information about the error by using Err Object.

 

Example

Applies To