GetPointAt Method
Returns the point at the given index.
Syntax
object.GetPointAt(lIndex)
Properties
The GetPointAt method syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
lIndex |
Long. The index of the point you want returned. |
Return Value
Object. An object of class FixFloatPoint, which contains the x and y coordinates.
Remarks
This function allows users to iterate through the data point array. The maximum index is determined by the number of data points in the object.