EnableTooltips Property

Specifies whether the tooltips are shown for the specified object.

Syntax

object.EnableTooltips [= Boolean]

Properties

The EnableTooltips property syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

Boolean

Whether the shape's tooltips are displayed.

Settings

The settings for Boolean are:

Value

Description

True

The tooltips for the specified shape are displayed.

False

The tooltips for the specified shape are not displayed. (Default)

Remarks

When EnableTooltips is set to True, the text displayed is the text set in the Description property for the specified object.

 

Applies To