To configure
I/O drivers to start automatically:
- In Classic view, from the iFIX WorkSpace, click the System Configuration Utility button on the toolbar.
-Or-
In Ribbon view, on the Applications tab, in the System & Security group, click SCU.
- On the SCU toolbox, click the Tasks button.
- In the Filename field, enter the full path of the I/O control task.
- In the Command Line field, enter the appropriate command line parameters. If you enter more than one parameter, separate each parameter with a space.
- In the Start Up Mode area, click the Background option button.
- Click the Add button.
- Click OK.