To add an I/O
Driver to the Configured I/O Drivers list box:
- In Classic view, from the iFIX WorkSpace, click the System Configuration Utility button on the toolbar.
-Or-
In Ribbon view, on the Applications tab, in the System & Security group, click SCU.
- On the SCU toolbox, click the SCADA button.
- Next to the I/O Driver Name field, click the browse (...) button to display a list of I/O drivers installed on the local node. The Drivers Available dialog box appears.
- Select the driver you want and click OK. The driver appears in the I/O Driver Name field.
- Click the Add button. The SCU adds the I/O driver to the Configured I/O Drivers list box. Only drivers added to this list box are started during iFIX startup.
NOTE: During installation, the Simulation (SIM) driver is automatically installed for you. This driver provides 2000 registers for simulating process data and testing your database. Refer to the Building a SCADA System e-book for more information on using the SIM driver.