Configuring the Alarm Startup Queue Service
To configure
the Alarm Startup Queue Service:
- In Classic view, from the iFIX WorkSpace, click the System Configuration Utility button on the toolbar.
-Or-
In Ribbon view, on the Applications tab, in the System & Security group, click SCU.
- On the SCU toolbox, click the Alarms button.
- Double-click the Alarm Startup Queue Service.
NOTE: The Alarm Startup Queue Service only appears in the alarm configuration list if networking is enabled in the SCU. To enable networking from the SCU, close the Alarm Configuration dialog box, and on the Configure menu, click Network. The Network Configuration dialog box appears. In the Network area, select the network type. Once networking is enabled, you can try to configure the Alarm Startup Queue Service again.
- In the Startup Queue Configuration dialog box, clear the Summary alarms only check box to receive alarms and messages. To receive only alarms from the Alarm Summary Service, leave the check box selected.
- If you want to filter alarms by time, select the Enable Time Filter check box and enter the maximum age of the alarms and messages you want to receive in the Hours and Minutes fields.
- Click OK.
See Also
Alarm Configuration Dialog Box
Startup Queue Configuration Dialog Box
Network Configuration Dialog Box
Configuring an Alarm Printer Service
Configuring the Alarm File Service
Configuring the Alarm History Service
Configuring the Alarm ODBC Service
Configuring the Alarm Startup Network Service