Configuring an Alarm Printer Service
To configure
an Alarm Printer Service:
- In Classic view, from the iFIX WorkSpace, click the System Configuration Utility button on the toolbar.
-Or-
In Ribbon view, on the Applications tab, in the System & Security group, click SCU.
- On the SCU toolbox, click the Alarms button.
- Double-click the Alarm Printer Service.
- In the Port Definition areas, click the option button for the printer port to which your printer is connected. Each port can handle only one Alarm Printer Service. If a port selection is not selectable, it is assigned to another printer.
- In the Printer Name field, enter a printer name.
- Select the printer's alarm areas.
- Select the printer's message format.